Create PLCopen Axis

To create a new PLCopenA vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML axis, follow these steps:

  1. In the Project Explorer, right-click on the PLCopen item and select the New Axis command in the menu
  2. Fill in the PLCopen Axis Data dialog
  3. In the Dictionary, right-click on the Global variables node and select the Add variable command in the menu.
  4. Create a new instance of the AXIS_REF data structure

    PLCopen Axis - New Instance of AXIS_REF

  5. Figure 5-18: PLCopen Axis - New Instance of AXIS_REF

  6. Then, this Axis Name (MyNewAxis in our example) is an instance of an AXIS_REF library function that can be used in your PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events programs

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™